2017-10-21 8:34 AM
Hello Everyone,
I'm struggling to setup communications between two 868 MHz sub-GHz modules.The first module is the STEVAL-IDS001V4M (USB dongle with SPSGRF-868) and the second module is the STEVAL-SP1ML868 (USB dongle with SP1ML-868). I'm using the Windows application 'SPIRIT1 DK Application v2.2.1' to configure the radio and packet settings of the STEVAL-IDS001V4M module, then using the 'Transmission Test' window to send the text 'Hello World'.The radio and packet settings for the STEVAL-IDS001V4M are as follows (configured via the GUI):
Frequency Base: 867.999967 MHzData Rate: 38.433 kbpsFrequency Deviation: 19.836 kHzChannel Filter: 102.115 kHzModulation: 2-FSKOutput Power: 0 dBmPacket Format: BASIC
Preamble Length: 4Sync Length: 4Sync Value: 0x88888888CRC: No CRCFEC: DisabledData Whitening: EnabledThe radio and packet settings for the STEVAL-SP1ML868 are as follows:S00:BAUD_RATE=115200S01:FREQUENCY=868000000S02:DATA_RATE=38400S03:MODULATION=0S04:OUTPUT_POWER=11.6S05:FREQ_DEVIATION=20S06:RX_FILTER=100S07:CS_MODE=0S08:RSSI_THRESHOLD=-130S09:PREAMBLE_LEN=4S10:SYNC_LENGTH=4S11:SYNC_VALUE=0x88888888S12:CRC_MODE=0S13:WHITENING=1S14:FEC=0S15:SOURCE_ADDR=0x00S16:DESTINATION_ADDR=0xffS17:MULTICAST_ADDR=0xeeS18:BROADCAST_ADDR=0xffS19:FILTER_CRC=0S20:FILTER_SOURCE=0S21:FILTER_DESTINATION=0S22:FILTER_MULTICAST=0S23:FILTER_BROADCAST=0S24:TX_RX_LED=1S25:RESERVED=S26:ESCAPE_SEQ=1S27:SOURCE_FILT_MASK=0x00S28:PAYLOAD_SIZE=32The data received from the STEVAL-SP1ML868 is:
ccy»{c#Something is being received but not 'Hello World'.
I assume the two dongles are compatible? They both use the SPIRIT1 module.
I'd be very grateful if anyone can help or provide any suggestions.
Mike.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.