2018-10-11 11:36 PM
Hi,
I'm fighting with a low data throughput of the BlueNRG-MS. The BlueNRG based device acts as a peripherial and sends notifications periodicaly to PC or Android app. The problem is I'm not able to achieve a higher data rate than approx. 1 kB per second. BLE frame data size is 20 bytes.
How should I increase the data speed? I think the way is sending multiple packets within one connection interval but I don't know how to do this. Or is there another way?
Thanks a lot
Zdenek
2018-10-19 10:47 AM
I was fighting the same problem a while ago. Here are the things we did to get the throughput up and get multiple packets sent in one connection interval:
Using these techniques, I was able to observe 2 to 4 packets sent per connection interval with a Bluetooth protocol analyzer.
If you need even more throughput, consider going to BlueNRG-2 with its higher MTU. With one big characteristic update, the L2CAP on the chip figures out how to pack the connection interval.
2024-11-21 12:36 AM
Hello,
I'm trying to achieve the same thing for a "SPBTLE-RF" module on a B-L475E-IOT01A2 Discovery Kit which is based on BluneNRG-ms. I'm trying to achieve a total baud rate of about 256 kbps.
I've tried multiple approaches like breaking the data down to multiple characteristics but I was not able to go higher than about 16kbps. However, in the datasheet for BlueNRG-ms, it says that the "Data Rate" can go up to 1 Mbps. I'm so confiused.
I would appreciate it if you could guide me in the right direction.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.