2015-07-13 7:57 AM
Which concurrent roles does the the BlueNRG-MS support?
For example: 3 Master - MyDevice2 Master - MyDevice - 1 Slave
1Master - MyDevice - 2 Slave
MyDevice - 3 Slave
Regards Thomas
#bluenrg-ms2015-07-20 5:51 AM
Dear Customer,
using the stack Mode4 (only for BlueNRG-MS), the device can be configured as:
- Master and Slave (up to 2 masters) - Simultaneous advertising and scanning - Up to 4 connections - 12 KB of RAM retention.Regards,
GMWhich concurrent roles does the the BlueNRG-MS support?
For example: 3 Master - MyDevice2 Master - MyDevice - 1 Slave
1Master - MyDevice - 2 Slave
MyDevice - 3 Slave
Regards Thomas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.