Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG: No HCI ACL Data

Posted on May 13, 2015 at 10:43Hello,now I have my STM32 up and running, communicating with a BlueNRG. But after the first connection event, I do not get any ACL data. With my BLE sniffer, I see an ATT ''exchange MTU request'', but I don't get any i...

torsten2 by Associate II
  • 1122 Views
  • 2 replies
  • 0 kudos

BlueNRG-MS concurrent role

Posted on July 13, 2015 at 16:57Which concurrent roles does the the BlueNRG-MS support? For example: 3 Master - MyDevice   2 Master - MyDevice - 1 Slave   1Master - MyDevice - 2 Slave   MyDevice - 3 SlaveRegards Thomas #bluenrg-ms

thomas by Associate
  • 844 Views
  • 1 replies
  • 0 kudos

SPWF01S

Posted on July 20, 2015 at 12:00hello, please excuse my limited knowledge here.  I am evaluating the SPWF01 module and have it connected successfully to an AP but I would also like it to open a SOCKD command on startup - it is not connected to a hos...

BlueNRG - Module planed?

Posted on May 23, 2014 at 11:00Hello Does ST plans in the short term to produce its own Bluetooth LE module using the BlueNRG controller? The BlueNRG controller does need quite a lot external components compared to its competitors (like TI ), sellin...

Tantalum by Associate II
  • 3547 Views
  • 7 replies
  • 0 kudos

How to define bidirectional GPIO pins in STM32?

Posted on July 09, 2015 at 11:57Dear all, I am using a high density STM32F103 MCU where I need to define GPIOC0-GPIOC7 as bidirectional since data on all these pins will either be sent or received to/from another chip. I have designed these pins as:...

danesh by Associate II
  • 3687 Views
  • 4 replies
  • 0 kudos

SPWF01 fails with multiple HTTP requests

Posted on July 15, 2015 at 08:43 Hi, I am hoping to be able to serve some web pages from the SPWF01 which make use of javascript and css. I have put some test files into the flash and they can be fetched using HTTP individually OK but when I try to ...

markb by Associate II
  • 812 Views
  • 1 replies
  • 0 kudos

Problem connection to AP

Posted on July 07, 2015 at 13:25Hi. I have a problem to connect the SPWF01SA1 with my Access Point. When the module try to connect restart before complete the Wifi scanning. Does anybody can help me. my config, status, & capture file as attachment. ...

n2399 by Associate
  • 1722 Views
  • 2 replies
  • 0 kudos

SPI connect to SPWF01SC

Posted on July 02, 2015 at 16:04Hi, I'd like to use the SPI connection of SPWF01SC. Could you say me please which pinout description are right? Is the the DocID025635 Rev 2 and the STEVAL-IDW001V1 with SPI description right? http://www.mikrocontrol...

christos by Associate II
  • 1235 Views
  • 3 replies
  • 0 kudos

[solved]fastest communication

Posted on April 20, 2015 at 11:29Hi,I'm trying to achieve a communication between two wifi devices through a SPWFO1SA.11 , and I want to achieve the highest possible bite rate. My questions are then:-Can I use the mentioned SPI port to perform the A...

hector by Associate II
  • 4414 Views
  • 12 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.