2017-03-31 1:32 AM
Hi All,
I am running BLE central and peripheral profile applications on Mentor Graphics Nucleus RTOS using two STM32 MCUs interfaced with BlueNRG-MS modules. BlueNRG-MS firmware version is 7.2a, STSW-BLUENRG-DK version is 2.01 and profile libraries have been used from OSXSmartConnPS package (V1.5.0).
The problem is that when I try to connect master and slave using any method for Temporary Key Calculation, the pairing fails and packets are not encrypted when seen from Wireshark logs while the same applications pair successfully when run in bare metal environment using NUCLEO-L476RG and
X-NUCLEO-IDB04A1 BlueNRG expansion board. The Wireshark logs for both the cases are attached. Any help in this regard will be highly appreciated.
Security parameters on central and peripheral sides used for pairing are as following:
:::PERIPHERAL SECURITY SETTINGS:::
ioCapability = NO_INPUT_NO_OUTPUT;
mitm_mode = MITM_PROTECTION_REQUIRED;bonding_mode = BONDING;OOB_Data_Present = OOB_AUTH_DATA_ABSENT;Use_Fixed_Pin = USE_FIXED_PIN_FOR_PAIRING;encryptionKeySizeMin = 8;encryptionKeySizeMax = 16;Fixed_Pin = 111111;initiateSecurity = SLAVE_INITIATE_SECURITY;:::CENTRAL SECURITY SETTINGS:::
IO_CAPABILITY = KEYBOARD_DISPLAY
MITM_MODE = MITM_PROTECTION_REQUIREDOOB_ENABLE = OOB_AUTH_DATA_ABSENTUSE_FIXED_PIN = USE_FIXED_PIN_FOR_PAIRINGFIXED_PIN = 111111 BONDING_MODE = BONDING#bluenrg-ms #bluenrg-pairing #bluenrg2017-04-03 2:05 AM
Hi Muhammad,
could you update the BlueNRG-MS FW to 7.2c and check again? You can do this using this
https://developer.mbed.org/teams/ST/code/BlueNRG-MS-Stack-Updater/
or version 2.0.2 of package. You should also update the profiles application using version 1.6.0 ofhttp://www.st.com/content/st_com/en/products/embedded-software/open-rf/osxsmartconnps.html
.Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.