2022-07-13 6:02 AM
Hello,
I am developing a platform with BLE Beacon connectivity and I am looking to extend the range of our device. Until now, I have been using BLUENRG-M2SA module, which is BLE v5.2 ceritifed. I know that BLE v5.1 >= versions include "long range" mode ( 125 or 500 kbps datarate ), usually described as Coded PHY, but couldn't find any mention of it on M2SA documents.
Does BLUENRG-M2SA module support BLE Coded PHY ? If yes, could you point me to a respective document or source file ?
Solved! Go to Solution.
2022-07-13 7:46 AM
It is often misunderstood that the Long Range Feature (Coded PHY) is not a mandatory part of BLE 5.x, but an option.
BLUENRG-M2SA is a module incl antenna based on the BlueNRG-2, which is compliant with BLE 5.0 but does not yet support Long Range. In the newer SoC BlueNRG-LP, a number of improvements were made, including Long Range (Coded PHY).
Does it answer your question?
Regards
/Peter
2022-07-13 7:46 AM
It is often misunderstood that the Long Range Feature (Coded PHY) is not a mandatory part of BLE 5.x, but an option.
BLUENRG-M2SA is a module incl antenna based on the BlueNRG-2, which is compliant with BLE 5.0 but does not yet support Long Range. In the newer SoC BlueNRG-LP, a number of improvements were made, including Long Range (Coded PHY).
Does it answer your question?
Regards
/Peter
2022-07-13 8:13 AM
Thank you Peter, that cleared it out
2022-07-14 8:43 AM
One last clarification @Peter BENSCH , BLUENRG-M2SA doesn't support Long Range (Coded PHY) for both TX and RX, is that correct ?
2022-07-14 9:54 AM
Correct, BlueNRG-M2SA does not contain the Long Range (Coded PHY) function, it was only implemented in the more recent BlueNRG-LP.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.