2020-10-06 1:58 AM
I have a BlueNRG-M2SA on a board with an STM32 Host. I can build and load projects onto the BlueNRG M0 using the SWD port with St-Link.
Next I tried to use the Bootloader via the Host - I have Host control of the Boot Pin, Reset & Uart.
I intended to use the Flasher Utility which I can connect to my Host, and wrote a simple Uart Relay to transparently transfer bytes between the Utility and the M0 via the Host. So the Flasher Utility thinks it is connected directly to the M0.
I assert the boot pin high and reset the M0 at the start to put it into Bootloader mode.
I tested the relay by using a terminal program to send 0x7F and receive back a 0x79 from the M0 - which is the start of the Bootloader Protocol according to AN4872.
However when I use the Flasher Utility it fails with "Auto Baudrate functionality failed" and does not appear to send 0x7F.
I note that this version of the Flasher Utility v4.0.0 does not provide the pop up
whereas the previous version, which is no longer available did.
I suspect this is the issue - how can i make the utility recognise I want Bootloader not normal flash read or write?
2020-11-11 2:03 AM
I also have the same issue: Flasher Utility v4.0.0 + BLUENRG-M2 - fails with "Auto Baudrate functionality failed". no pop up window with UART settings. When I use console and send 0x7F Bluenerg-M2 responds with 0x79.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.