2024-07-31 9:46 AM
I'm trying to follow the test procedure for BlueNRG-MS (SPI) indicated in the Bringing up the BlueNRG and BlueNRG-MS devices - Application note (AN4494).
I am using custom board (Microchip dsPIC33F) to talk to BlueNR-M0A.
SPI Setting: 625K baud rate, SPII mode 0.
Following the Test procedure on Page 5, I got correct packet from BlueNRG-M0A:
Step 4: I received [02,7F,00,00,00]
Step 6: I received [02,7F,00,06,00]
However, on Step 7, I always received [FF, FF, FF, FF, FF, FF]. Note: I sent CTRL byte 0x0B, followed by 4 dummy byte 0x00.
I have checked codes again and again, have no idea where to look at.
Please help with this issue, and point out a direction.
Thanks.
Leo
Solved! Go to Solution.
2024-08-05 7:31 AM
Hi Barry,
I did quick test to verify the issue was caused by CS line staying LOW too short.
1. I changed SPI baud rate to 312.5K which I will use on final firmware, Tclk = 3.2us.
2. Set Delay_us(10) between CS Line HIGH and LOW: last step always returned 0x00
3. Set Delay_us(30) between CS Line HIGH and LOW: on last step, most returned right [04, FF, 03, 01, 00, 01], a few response incorrect. Note: I put a while loop on the test, so it will repeat from Step 1 to 7.
4. Set Delay_us(45) between CS Line HIGH and LOW: all returned right.
Note: Delay_us() function has tolerance on delay microseconds. Delay_us(45) will make sure the delay > 32us.
I think that's it. I will move forward on my project.
Thanks,
Leo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.