Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STKNX Buck converter don't get 12V output

I am trying to get 12V at the output of STKNX buck converter, but I am not getting it and the STKNX dead.The RFB1 that I am using is 33K Ohm and the RFB2 is 3k Ohm, with these resistors the Vout would be 1 + 33k/3k = 12V. The maximum value of this vo...

IO-Link slave protocol stack for object-oriented programming portable to any MCU platform,portable IO-Link communication master station

Background:        I have implemented an IO-Link communication slave device using IO-Link PHY chips such as L6362. After multiple rounds of object-oriented code organization。The MCU resource driver, IO Link slave protocol stack, and PHY chip were abs...

STEVAL-IDP004V2

Hello, I am experiencing issues with my STEVAL-IDP004V2 evaluation board. When I connect the device to my  computer, it is not recognized properly. Attempted to update the USB drivers through device manager, used different USB ports and cables. Where...

bobrzyn by Associate
  • 959 Views
  • 0 replies
  • 0 kudos

Dev.Kit STEVAL-BFA001V2B - IOLink

Hi,I am testing the STEVAL-BFA001V2B development kit to evaluate the use of the IOLink protocol. Using the native project provided in the software package for the STide development environment, the device connects to the master and works correctly. T...

padovmar by Associate
  • 854 Views
  • 0 replies
  • 0 kudos

Resolved! STW81200 does not answer on MISO line

Hi, Im interfacing STW81200 with SPI without no success. I do have the following questions:What the SPI mode? Its not clear on the datasheet. It seems that CPOL = 1, and CPHA = 1.In either way, I have tested the communication with several modes and n...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.