2022-08-09 8:04 AM
Hello there
I have a custom board based on STEVAL-IDB011V2 EVM. Is the same schematic but I have a problem with this. Apparently it boots but not run...
When I flash "Hello World" example I have some issue that I can't check why.... The expected message does not is sent complete. So I have this output:
In this test, I reset the board sometimes. Some times it shows "Applicat", "Applicati", (Probably bootloader output?) Some times it shows truncated "Hello World".
I checked voltage levels by https://www.st.com/resource/en/application_note/an5503-bringing-up-the-bluenrglp-bluenrglps-devices-stmicroelectronics.pdf application note (bringing up the bluenrglp devices).
I tried the Power Supply test (flashing DTM Firmware - UART without update) and VDDA thats we expect 1.2V, I measured 0V. The Core voltage (VCAP) I measured 1.2V as expected.
I also tried flash other firmware examples without success.
Can someone help me?
Solved! Go to Solution.
2022-08-18 12:53 AM
Hi,
I just replied to your message.
I guess the problem was related to 22nH used for SMPS instead of 10uH (22nH is optional and can helps in sensitivity performances - "killing" the SMPS spurious).
Please confirm.
Regards
Laurent
2022-08-17 12:31 AM
Hello,
Could you share your schematics and associated Bill of material?
Regards
Laurent
2022-08-17 1:51 PM
Hello there
Please see you message inbox. I sent to you.
Regards,
Leonardo Trinta
2022-08-18 12:53 AM
Hi,
I just replied to your message.
I guess the problem was related to 22nH used for SMPS instead of 10uH (22nH is optional and can helps in sensitivity performances - "killing" the SMPS spurious).
Please confirm.
Regards
Laurent
2022-08-18 6:29 AM
Hello there
Yes, was it that's what caused the issue. Sorry for inconvenience.
As suggestion, clarify it in EVM schematic.
Thank you
Regards,
Leonardo
2024-01-09 11:36 AM
Hi Laurent,
I just saw this post and I'm wondering if I have an issue with my schematic as well.
Based on schematic for STEVAL-IDB011V2, there is a 22nH inductor for L4 (attached to VLXSD) and based on the datasheet DS13282-rev-6, page 11, I have a similar thing, VLXSD->22nH->(VFBSD and (4.7uF || 0.1uF) caps to ground.)
I do not have a 10nH inductor in series with the 22nH inductor as shown in the V1 schematic of UM2735 page 99). Will this cause issues with SMPS ON operation?
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.