2019-06-12 5:43 AM
I am trying to program BlueNRG-2 device with low level radio APIs. Every time a packet received with crc error, the time schedule of the communication is disrupted, since the time is random for packets with crc error. I wonder how to disable the interrupt generated by packet receive with crc error.
Thanks
2019-06-12 6:20 AM
By the way, how to initialize the timer which is used to capture the timestamp of the received packets? The timer is 24bits and based on 512kHz clock.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.