Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How update MTU size for Bluetooth?

Background: I have written Embedded application running on a STM32 chip with BlueNRG_M0 Bluetooth(4.2) LE module. I have a C# windows Application that is the client and is reading data form the embedded(remote) device. Problem Statement: The C# is on...

DKopp.2 by Associate III
  • 1486 Views
  • 0 replies
  • 0 kudos

Hello every one, I'm using BlueNRG-m2 to communicate over ble, I make an interface with blueNRG over spi from stm32f446 mcu, my problem is that the ble linked list used in ble stack seems like it doesn't initialized correctly.

when I try to read software version (before gap or gatt initalization) using aci_hal_get_firmware_details(), it ends up to this and always fail to get the data correctly

_legacyfs_online_stmicro_images_0693W00000bhdrnQAA.png

RTOS example with X-CUBE-BLE2 BlueNRG M2

I using BlueNRG M2 as a network co-processor and have configured my project with STM32 CUBEMX which uses X-CUBE-BLE2. It is a non RTOS based project and is working well.Now, I want to use RTOS (FreeRTOS) with the BLE stack. Is there any example which...

RMoc.1 by Associate II
  • 881 Views
  • 0 replies
  • 0 kudos

2nd SPIRIT1 does not transmit

Dear Community,I have a setup of 2x SPIRIT transmitters. The CSMA is disabled. Both are configured for continuous TX. However, I observe the following:1) The SPIRIT that boots initially starts transmitting without any issues2) The second SPIRIT (that...

VMeto.1 by Associate II
  • 1466 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.