Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLE_STATUS_TIMEOUT with terminate_gap_procedure

Hi everyone,I am developing an IOT solution using the BLUENRG-M0 from ST.I am coding in C and I use a custom board with SPI communication between the BLUENRG and my MSP430F5255 from T.I . I am using the ACI API to transmit commands to the BLE module....

GBara.3 by Associate II
  • 3745 Views
  • 11 replies
  • 0 kudos

I purchased the STUSB4500QTR and actually operated it. After assembling the electronic board, I dumped the default contents of the register and it became as shown in [1A] below. Next, when I purchased parts from a new lot during mass production and assemb

*********************************************************************************(Contents of register [1A])0xC0: 0x00 0x00 0xB0 0xAA 0x00 0x45 0x00 0x00 0xC8: 0x10 0x40 0x9C 0x1C 0xF0 0x01 0x00 0xDF 0xD0: 0x02 0x40 0x0F 0x00 0x32 0x00 0xFC 0xF1 0xD8...

ODais.1 by Associate
  • 1354 Views
  • 0 replies
  • 0 kudos

Hi I am implementing a nrf24l01 driver with the use of stm32F4 the SPI transmit and receive works with the polling method yet not with DMA method.I already configured the DMA on cube mx and IAR WORKBENCH this is the code part i put the dma as cmnt

//3. Read single byte from a registeruint8_t NRF24_read_register(uint8_t reg){   uint8_t spiBuf[3];   uint8_t retData;   //Put CSN low   NRF24_csn(0);   //Transmit register address   spiBuf[0] = reg&0x1F;   HAL_SPI_Transmit(&nrf24_hspi, spiBuf, 1, 10...

atoua.1 by Associate
  • 1446 Views
  • 0 replies
  • 0 kudos

Resolved! HAL_transmit in other fils (no main.c)

Hello,I'm trying to send data over uart from a another file.My main :UART_HandleTypeDef huart1; DMA_HandleTypeDef hdma_usart1_tx;   int main(void) { MX_USART1_UART_Init();   While(1) { } }My error is :../Core/Src/AT_Command.c:22:2...

jlecl.1 by Associate III
  • 2017 Views
  • 2 replies
  • 0 kudos

Unable to load the firmware

Hi, first of all i'm a noob with bluenrg products,I'm using the STEVAL-IDB008V2 and i'm able to load firmware using the RF-flasher utillity via COM port identified as ST DK just fine, but when i try to load the same firmware using a standard com por...

_legacyfs_online_stmicro_images_0693W00000bVh83QAC.png
A.Presm by Associate
  • 1028 Views
  • 0 replies
  • 0 kudos

ST8024CDR . Are support smart card ( ISO 7816-3 Integrated Circuit Card (ICC) Digital Controller) reset synchronous and asynchronous

Please help i need to know about. Smart card interface ST8024CDR it can support Smart card ISO7816-3 in reset mode synchronous or not ? Now i using this ic it support only asynchonously asynchonously reset timming diagramsynchonously reset timming d...

_legacyfs_online_stmicro_images_0693W00000dK32VQAS.png _legacyfs_online_stmicro_images_0693W00000dK32kQAC.png
Nunut by Associate
  • 1001 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.