Drop in Replacement for ISP1763AHNUM
Dear Support,Please help to check and advise drop in replacement for ISP1763AHNUM?Thanks
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
Dear Support,Please help to check and advise drop in replacement for ISP1763AHNUM?Thanks
Hi everyone, I hope everyone is doing fine in these challenging times. I am trying to develop a new product range based on the BLE MESH network for which I have selected the BlueNRG-LP family to go with.I have downloaded the latest mesh software stac...
Hello ST-CommunityI have a little problem with bluenrg-2m, I'm handling the the user event process in 100ms RTOS timer call back with stmn32f446.The problem is when I send a file using mobile app call bluetooth terminal, It become too slow !1kbyte pe...
Hi,I want to rearrange the generated files of peripherals and protocols(like usart.c, tim.c, adc.c) from the core folder to the driver's folder and rename the core folder to the Application. Is it possible in stm32cubeIDE?ThanksMathan
My customer installed some sites with cards with S2-LP (one central board and one remote).On a particular location the S2-LP crashes. Now I'm searching the problem but while I'm searching I would like that the customer resets the S2-LP (not the entir...
Hi,I have a custom PCB based on STM32L4R9 with a SPI interface to BlueNRG-2 flashed with DTM SPI (2.1f stack). I use X-CUBE-BLE2.I'm able to communicate with the module such as retrieve firmware details, start and stop tones. The problem I'm seeing i...
Using WiSE-STUDIO and BlueNRG SDK 1.4.0 on Windows 11Debugger is USB to the board, configured as CMSIS-DAPI'm able to flash code to the board, but I cannot see an option for "Live Expressions" anywhere. Is this not supported?
Hi,I notice that the STHV series chips have T/R switch in it, but I wonder if the evaluation board can receive the echo signals? Then, if I want to develop a PCB board with STHV series chips, do I need to add a waveform generator before STHV chips?...
Hello,I'm from Viet Nam,I am currently working on a project to use eSIMs for electronic meters.Can you show me how to bootstrap VNPT's profile to your eSIM chip? (VNPT is a major telecommunications corporation in Vietnam)Best Regard!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.