Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP Registers

Hi Everyone,I have some questions regarding the registers of the Sub-1GH transceiver 'S2-LP':1) Which registers (configuration registers) are retained in "standby state", in "sleep_A state" and in "sleep_B sate"? Which registers are not retained, and...

WN by Associate
  • 1222 Views
  • 2 replies
  • 1 kudos

Transmitter and receiver address, s2-lp

Hi, Is it possible to set the address of the transmitter or receiver via S2_LP DK? My project involves sending data via s2-lp between two sets (nucleo-l053r8 with steval-fki868v2), I would like to set one for receive only and the other for read only....

DanielH by Associate
  • 1432 Views
  • 1 replies
  • 0 kudos

Issue when compiling BlueNRG-2 SampleApp

Hi,I'm trying to compile the example called SampleApp using keil uVision as IDE. When the project is created, in the Manage Run-Time Environment, the Startup selector in the Device tab is not selected by default, but I selected it before compiling th...

1.jpg 2.jpg 3.jpg
dsm85 by Associate
  • 1280 Views
  • 1 replies
  • 0 kudos

BlueNRG0 optimizing BLE troughput.

 Hello,I am an engineering student currently working with the BlueNRG-M0 for a student project. My setup consists of a mobile application communicating with embedded firmware through the BlueNRG-M0. However, I'm facing an issue: the throughput is qui...

Reda by Associate
  • 748 Views
  • 0 replies
  • 0 kudos

Optimizing Bluetooth LE

 Hello,I am an engineering student currently working with the BlueNRG-M0 for a student project. My setup consists of a mobile application communicating with embedded firmware through the BlueNRG-M0. However, I'm facing an issue: the throughput is qui...

Reda by Associate
  • 1015 Views
  • 0 replies
  • 0 kudos

Configuring STM32U575 for I2C DMA transfer

I am working through a workshop tutorial on how to configure and use GPDMA transfers via the linked list functionality provided in STM32CUBEMX. When setting the linked list runtime configuration a Source Address, Destination Address and Data size are...

ITayl.1 by Associate
  • 2101 Views
  • 0 replies
  • 0 kudos

Resolved! ST4485EB : is it 5V compatible

Hi,The ST4485EB IC mentions that it needs a 3v3 supply. How can we ensure that the A and B lines interoperate with other RS485 devices working at a 5V logic level as the datasheet mentions . Should I just provide 5V supply to this chip so that it int...

Nilav_1-1697524248396.png Nilav_0-1697524168920.png
Nilav by Associate II
  • 2444 Views
  • 4 replies
  • 2 kudos

VNH5180A-E

i have buy VNH5180A-E powersso-36 tp pakage some 20pcs but i check measurement not as per datasheetcan you let me knowdimension A /a2 = 2.53 mm  as per our  ( as per datasheet is 2.15-2.47mm)dimension H = 9.91 mm as per our ( as per datasheet is 10.1...

peter_hk by Associate
  • 819 Views
  • 0 replies
  • 0 kudos

Resolved! How are the BLE attribute handle offsets defined?

Where can I find documentation on the BLE attribute handle offsets? I was adapting code from the sensor demo for the BLE NRG 2 and am trying to understand the "aci_gatt_attribute_modified_event" callback. Through observation and experimentation I fou...

BPaik by Senior
  • 5601 Views
  • 11 replies
  • 6 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.