Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST67W61M1 Connection Errors and DTIM Issue

Hi,I am currently working on a feasibility project using the X-NUCLEO-67W61M1 and NUCLEO-U575ZI-Q.The sample code I am using is ST67W6X_FOTA.The FOTA functionality is working properly. However, during the initial connection phase, there is about a 50...

Jerrylin00_0-1776060565581.png

Resolved! Unable to bring up ST67

Hi,1. [Part Number] STM32H7R7I8T6 2. [Environment] x-cube-st67 1.2 version and latest cube IDE.3. [Schematics] If it is a custom board --> Share the schematics using “Attach file” option or inserting some image.4. [Details] I am using STM32H7R7I8T6 M...

JohnWick1 by Associate II
  • 962 Views
  • 10 replies
  • 5 kudos

STPM34 critical component analysis

We are pursuing UL3141 for Power Control Systems (PCS), this includes UL991 which is the Standard for Tests for Safety-Related Controls Employing Solid-State Devices, and it requires a critical component analysis. In our particular design, the STPM34...

Resolved! S2-LP PERS_RX - what does it do?

The function of the PERS_RX flag in PROTOCOL 0 is described as: '1: enable the persistent RX mode.' What does that actually mean/do? I couldn't see any explanations in the rev. 13 data sheet for the S2-LP. 

kzkaram by Associate II
  • 415 Views
  • 4 replies
  • 1 kudos

BlueNRG-1 Driver for SSD1306

Hi, Here i post a driver for SSD1306 128X64 Oled Display. You must enable I2C configuration void I2C_ConfigurationMaster(void) { GPIO_InitType GPIO_InitStructure; I2C_InitType I2C_InitStruct; /* Enable I2C and GPIO clocks */ if ((I2C_Type*) SDK_...

Diltech by Associate II
  • 162 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.