Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Add a USB host port on a STM32F103 dev board

Hi, I'm just starting out with embedded programming & electronics so please bear with me :)I am starting a project based on the STM32F103 Nucleo board. The first thing I want to do is create a USB host port to connect a class-compliant MIDI device.Fr...

0x80 by Associate
  • 5528 Views
  • 4 replies
  • 2 kudos

BlueNRG-M2 Bootloader from Application Code

I'm using the BlueNRG-M2 as my processor on an enclosed system with UART communication. My goal is to add the ability to update the firmware via this connection using the built-in bootloader.Using this answer, I am able to activate the bootloader wit...

lerneret by Associate
  • 867 Views
  • 0 replies
  • 0 kudos

S2-LP RAW DATA OPTION

Hello,In different project with S2-LP we want to read raw the for understand and anlyze any data of the communicate between 2 devices.Are we take tke raw data?Is the S2-LP support E527 standart?Thanks Melih

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.