2019-06-02 11:03 AM
Hi,
I'm just starting out with embedded programming & electronics so please bear with me :)
I am starting a project based on the STM32F103 Nucleo board. The first thing I want to do is create a USB host port to connect a class-compliant MIDI device.
From this link I learned that means the USB class is likely OTG. What I don't understand yet is what I need in terms of hardware. I would like to use a USB type A port. Can I hook it up straight to the MCU pins on the dev board without additional ICs?
I ordered this book today which will surely help me with this, but it will take some days to arrive and I'd like to prepare already if I can.
2019-06-03 2:20 AM
I think I've learned two important things this morning:
From what I've read here USB host / on-the-go class would require a 105/7 board at least. Luckily I didn't buy the hardware yet :)
That's a bit of a bummer because I was going base my project on an open-source project which uses the 103. I guess I will have to put in a bit more effort to port that code/hardware design.
But anyway, eventually my project requires both a USB host/OTG and a USB device port (also for MIDI) simultaneously. So I will first figure out that processor supports that...
2024-05-07 9:26 AM
Hi,
I am also having some trouble getting a USB breakout board connected to the Nucleo-F103RB, I only need the device in peripheral mode so not worried about otg, but I only get USB Device not recognised on my pc. I am still new to STM32 and this is the first time I am prototyping my own board for the chip, so I need to know how to communicate with the chip and instead of just buying the bluepill or similar as some have suggested for this issue.
2024-05-07 3:21 PM
Pull a schematic for the board and look at how the USB connects to the STM32F103 providing the ST-LINK functionality
Look at this, README.md explains wiring expectations
And these you might port over
2024-05-08 1:27 AM - edited 2024-05-08 1:32 AM
This is helpful, thank you. I was looking at the bluepill schematic originally and I have the wiring setup correctly as far as I can see, so I will try these repos and see how I get on. :smiling_face_with_smiling_eyes:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.