Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPIRIT1 stucks in READY state

Posted on June 27, 2015 at 00:17We have trouble to get the SPIRIT1 on our own board working. The very basic problem is that the chip can not be switched to any other state then ready Therefor the setup for any frequency settings are not possible. We...

ralph23 by Associate II
  • 2856 Views
  • 6 replies
  • 0 kudos

Socket response time

Posted on June 25, 2015 at 15:29Hi,I'm trying to set up a communication between two SPWF01SA.A is set as the server, B as the client. I wrote a text to send from A to B when the WIND 61 + WIND 60 are detected. If a try to do it just after the WIND 6...

hector by Associate II
  • 1248 Views
  • 3 replies
  • 0 kudos

Bluetooth scatternet

Posted on June 26, 2015 at 09:40I wish to create a bluetooth scatternet. The network consists of 15 nodes (microcontroller and bluetooth module). 3 piconets (maybe more) with 5 nodes . 1-4 nodes are connected to 5 node, 5-9 nodes are connected to th...

roomanaz by Associate
  • 1030 Views
  • 0 replies
  • 0 kudos

SPIRTI1 + SKY66100-11 power consumption

Posted on April 28, 2015 at 11:13Hi, I'm testing a solution with Spirit1 + SKY66100-11 for 169MHz transmission. I have a 600mA current consumption with spirit1+sky 66100-11+TCXO. Is it normal? Where Can I found a detailed technical report of current...

mauro by Associate
  • 1917 Views
  • 5 replies
  • 0 kudos

SPIRIT1 unknown state

Posted on June 11, 2015 at 22:10Hi Gaetano, I'm currently working with the SPIRIT1 on a my own board. An external clock signal is used on XIN coming from my MCU (STM32F4) at 26 MHz. And the central frequency is set to 868.3 MHz. Sometimes, I get an ...

SPIRIT1 register DEVICE_INFO content

Posted on June 15, 2015 at 15:20Unfortunately the data sheet can be evaluated as a minimum documentation for this chip. Is there any more information available e.g. for the DEVICE_INFO register, what the content is and could be and what it is tellin...

ralph23 by Associate II
  • 599 Views
  • 1 replies
  • 0 kudos

WEP in AP mode

Posted on June 15, 2015 at 12:34Is there a limitation/restriction of of the WEP key lengths in AP mode?Set password to 'test1': AT+S.SCFG=wifi_wep_keys[0],7465737431 AT+S.SCFG=wifi_wep_key_lens,05 This works OK.  I can connect fine with WEP authenti...

toby by Associate II
  • 1271 Views
  • 2 replies
  • 0 kudos

STW81200 Schematic / design guidance

Posted on June 11, 2015 at 12:22I am wanting to include the STW81200 into a new product design. I am looking for the schematic for the evaluation board that I think exists, but I am not able to find it.The specific information that I am looking for ...

Create a connection between three SPWF01SA

Posted on June 10, 2015 at 08:37Hello, i want to create a connection bettween three SPWF01SA an send data via TCP - socket to any other module. Is there a possibility to create something like that. The firmware is 150410-c2e37a3-SPWF01S. Thanks and ...

menyu1 by Associate II
  • 2292 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.