ST BLE Sensor App for Android
ST BLE Sensor 5.2.4 is closed once "Blue Voice Full Duplex" is selected. Below error message shown.
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
ST BLE Sensor 5.2.4 is closed once "Blue Voice Full Duplex" is selected. Below error message shown.
The IO-Link Master (multiport-hub) M12 port on the STEVAL-IDP004V2, has threads on the outside and is female on the inside.The M12 on the STEVAL-IDP003V1 has threads on the outside, and pins on the inside. Both are 4 or 5 pin compatible. I need cabl...
Hi,I'm beginner in USB-C and USB_PD some things are not clear for me.We developing a device which is a USB SLAVE Device - not HOST (Virtual comport device - datalogging to a notebook)This device has a large battery, so we want to charge the notebook ...
我尝试使用 STM32L4R9 与 AD7768 通信,使用 8 个通道。我想知道的是:是否可以使用 DCMI 建立 AD7768 与微控制器之间的通信(微控制器支持,但我不确定 AD7768 是否支持 DCMI。)如果 AD7768 也支持,我想知道 PCB 应该如何正确布线。Translation to English I am trying to communicate with the AD7768 using the STM32L4R9, using 8 channels. What ...
Hi, We try to use STPM34 to measure DC power besides measuring AC power. We had to disable the HPFs of V1,V2/C1,C2 on the EVALSTPM34 board by sending {0x00, 0x01, 0x18, 0x04, 0x88} and {0x02, 0x03, 0x18, 0x24, 0x92} to STPM34 through SPI. When we...
Hi, We try to use STPM34 to measure DC V and I inputs besides measuring AC. The HPFs of V1,V2/C1,C2 on the EVALSTPM34 board were disabled by sending {0x00, 0x01, 0x18, 0x04, 0x88} and {0x02, 0x03, 0x18, 0x24, 0x92} to STPM34 through SPI. ...
Background:Our project utilized ST's IMU sensor LIS3DH, and according to business requirements, we used click interrupt and initial interrupt respectivelyThe sampling frequency is 10HzWe set the duration of the Initial interrupt to 120 to generate an...
Posted on May 14, 2014 at 19:25Hi, My Interesting is the next, how can I use Spirit1 Auto retransmission and auto ack abilities in half duplex communication. My coordinator is supplied with main power, but nodes are powered by alkaline batteries. Th...
Hi everyone,I've recently using the BLUENRG-LPS chip for transmitting and receiving data, and I need to store the data from the chip directly into the SD card. Does the BLUENRG-LPS have the SD card driver?I found the STML4xx SD card driver in the Blu...
I currently have a BLUENRG-M2SP connected via SWD to my STLink-V3PWR.The issue is while my flasher can connect to the device it then cannot read the bootloader sector or flash the address memory.Here is the log:16:34:35.247: Waiting device to read bo...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.