2016-07-25 12:33 AM
We are attempting to use (and modify) the web interface of the module to configure it to connect to a certain SSID. The WiFi we are currently working towards have an SSID with a blank space in it. When using the web interface this results in the module trying to connect to a WiFi with the format Wifi%20Name rather than its real name, Wifi Name. The blank space does not seem to transcend into the module, it parses it as its actualy characters. Anyone have a solution for this?
Regards,Pontus2016-07-27 2:22 AM
Hi Pontus,
browsers automatically translate special characters to %something. Example above: ''...WiFi%20Modules/NewForm.aspx?RootFolder=%2fpublic...''You can enable decoding feature on module by ip_use_decoder configuration variable. Update to FW3.5.Regardsjerry2016-07-28 3:52 AM
Ok Jerry, thank you, I will attempt that.
However, when using captive portal and fill out the form I always get +WIND:57:Forbidden. How do I solve this?regards2016-07-28 4:29 AM
Got past that issue. But what decoding should be used when configuring from the captive portal? It actually makes it ''Wifi+Name'' rather than ''Wifi%20Name''. I have though modified the URL that is being created (captiveportal.net/firstset.cgi?SSID=Wifi%20Name .. etc) to try both + and %20. Neither of the tested decoding settings does anything to decode either of those. I have tried 1,2 and 6.
2016-07-28 10:15 AM
Hi,
it's not clear what's the issue. When firstset form is filled, module's cgi will automatically decode %something characters. Do you want to bypass default firstset.html, and implement your own firstset-like page?FYI: decoding function is used both from firstset cgi and output.cgi. You can use output_demo.html page to test incoming encoded strings, and decoding functionality based on different configuration variable values.- 1 means ''68656c6c6f20776f726c64'' becomes ''hello world''- 2 means ''hello%20world'' becomes ''hello world''- 6 (2+4) decodes html entities (''&#number;'' becomes a character)Regardsj2016-07-28 11:35 PM
Hello.
I am currently only using your pre-existing functionality. So by setting module to miniAP, connecting to its WiFi and going to captiveportal.net I come to the SPWFS01 First Config. So without modifying these files in the module I would want to use them, leaving potential modification until later. However, these are my issues:* Firstly, if I just fill out the form and click GO it does not work due to Authentication failed. I need to remove certain keys from the request to get rid of this.* If I fill out an SSID with a space in it, lets say WiFi SSID, it will be decoded into WiFi+SSID. This will not be decoded by module.* If I manually alter the URL (parameters after firstset.cgi?) to make it WiFi%20SSID and use ip_use_decoder = 2 this is still parsed by the module as WiFi%20SSID:+WIND:57:Received SSID is WiFi%20SSIDand the module is therefor not able to connect to the AP. So my obvious issue is that the module does not seem to attempt any decoding, no matter its configuration. If it is not possible we will have to sort this out differently.Regards
2016-07-29 9:24 AM
- Authentication failed means that inserted password is wrong (different from user_desc config var). There is no need to ''remove certain keys''. Simply, use the right password;
- If ''WiFi SSID'' becomes ''WiFi+SSID'', probably you/browser is not sending a ''%20'', and, so, cannot decode a ''space''. This is why in step 3 you alter the URL to force a %20. In step2 you/browser is not sending ''%20'', but ''+'';
- I expect ''%20'' is decoded as ''space''. This is what I see, also using output_demo. Please copy here configuration and status dump (AT&V and AT+S.STS).
Regards
jerry
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.