Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG2 aci_gap_init

Hello,  I use the STEVAL-IDB008V2 and I updated the BLE stack to v2.1f. Since this update I have an error when calling the aci_gap_init api. Please find below the sequence when I use an older stack    SEND => ACI_GAP_INIT_OPCODEParameters:| GAP Role ...

MBRAI.9 by Associate
  • 2635 Views
  • 2 replies
  • 0 kudos

BlueNRG-2

Hi,Please help if possible.I have an automotive electronic board which has a BlueNRG-2 device on it and it runs Yocto Linux on its main processor which is connected to the Ble chip via UART interface. I have loaded the the BlueNRG-2 device with DTM f...

RAlma.1 by Associate III
  • 4128 Views
  • 9 replies
  • 0 kudos

EVLKST8500GH-2 test envirionment

I am doing g3-PLC test by connecting two board of EVLKST8500GH-2  according to ST G3-Hybrid PLC&RF GUI Quick start guide, but i am not clear test envirionment 1) COM port of PC is connected with ST8500GH-MB or  NUCLEO-G070RB, when i connect with  NUC...

Resolved! ST60 Development Details

Hi, I have some questions regarding the ST60x parts Do you have a bulk quantity price estimate for the ST60A2 and ST60A3H1 parts? Are there recommendations for transmitting parallel data across the chip, such as preferred serializer/deserializer ICs?...

S2-LP Parameters configuration

Could someone help to understand the better value to use at frequency deviation, considering at bellow specs:   #define BASE_FREQUENCY 916000000 //Hz #define MODULATION_SELECT MOD_2GFSK_BT05 #define DATARATE ...

LPrat.3 by Associate II
  • 1372 Views
  • 0 replies
  • 0 kudos

Resolved! S2-LP - Interrupt flag problem

Hi,Some time ago I wrote a software with some changes from this library and successfully tested it with the STEVAL-FKI868V1 board and a ST board (STM32F779 EVAL).Now I made my own hardware with a little changes in the microcontroller pins. Communicat...

S2-LP.png
Slh by Senior
  • 1804 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.