Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Write SD card using bluenrg 332ac

Hi,I am trying to write the IQ data to the SD card (i.e., write the received CTE pkt to the SD card). However, I found that Bluenrg-332ac has a cortex M0 core, which may not be able to drive an SD card. Is it possible to use this cortex M0 core for S...

JasonYang by Associate II
  • 1990 Views
  • 3 replies
  • 2 kudos

54AC164245 and 5962R9858008VZC

Hi I'm using this device in a space design.  I just want to clarify the voltage requirements.  In all cases, I have Vdd1 >= Vdd2, as specified.  However, I'm using the device in these configurations and I want to confirm that the voltage levels are v...

rpmiller by Associate
  • 1897 Views
  • 3 replies
  • 0 kudos

PCB Layout for S2-LP

Hi I'm looking for a PCB Artwork file for the S2-LP transceiver with 915MHz Band. If you have any related materials or examples (like as PCB Job file or PCB Artwork file etc..,), please share them. Thanks a lot.

ChrisYu by Associate
  • 1259 Views
  • 1 replies
  • 0 kudos

Getting GNSS NMEA output from X-NUCLEO-GNSS1A1 software library between X-NUCLEO-GNSS1A1 board and B-L475-IOT Discovery board on serial terminal through UART comm protocol.

Following the "getting started doc" instructions: stacked the X-NUCLEO-GNSS1A1 to the B-L475IOT1A1 Discovery board through the Arduino UNO R3 connectors, opened and compiled the example application using STM32CubeIDE, dragged and dropped the binary p...

MChav.13 by Associate II
  • 1264 Views
  • 1 replies
  • 1 kudos

Resolved! EVAL-SCS001V1

I am hoping to understand whether or not this STUSB4500 PD controller on this evaluation board will default to a 5V sink level if it attaches to a standard USB-A port that does not communicate over the CC lines. I have tried this with a USB-C PD sour...

marke by Associate
  • 919 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.