Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-MS attribute handle in received event

Posted on April 23, 2018 at 07:03Hi all,I was able to port Environmental Sensor Service program to an STM32L4 MCU and the program seems to work fine with BlueNRG-MS application on smart phone.While going through the code, I came across that when the...

BlueNRG-1 pairing by pressing a button

Posted on April 16, 2018 at 15:31Hello!I am searching for the simple way of pairing on BlueNRG-1 by pressing a button on device.We have a device, which has no keyboard and display, only some buttons. We want to enable/confirm pairing on this device ...

Module soft reset

Posted on April 04, 2016 at 10:15Good morning to all,  I have a little problem with my module. After a filesystem update I send the command AT+CFUN=1 to reset the module. The module return OK, return ''+WIND:2:Reset'' but don't resect. Why?Stefano ...

stefano23 by Associate II
  • 6342 Views
  • 12 replies
  • 0 kudos

community.st.com

Posted on March 22, 2018 at 16:00SPBT3.0DP2 Tx buffering Hello,I'm evaluating the SPBT3.0DP2 as a replacement for an AMBER AMB2300 module, which is used in a RS485 to Bluetooth converter device designed around 2007. This converter is used to communi...

RS232 Communication

Posted on April 17, 2018 at 16:53Hello,I have a STEVAL-FKI868V1 based on a Nucleo L152RE board and i would like to connect a RS232 to my RX pin to get the information and then send it when i click on the button.So my main problem is about the code t...

BLUENRG1 notification enabled

Posted on April 16, 2018 at 17:00Is there a way to enable the feature notification when connection with the BLUENRG1 module took place? By default, the notification in module is disabled and can be turned on only from the PC.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.