2018-09-12 10:52 AM
Hello, I recently buy a new Nucleo-L4R5ZI-P board and I am trying to use it with the X-NUCLEO-IDB05A1 expansion board to develop a BLE application but it is being really stressful because although I am following the guide "Getting started with the STMicroelectronics BlueNRG-MS software package for STM32CubeMX", with the SensorDemo example, I cannot achieve it and in the Bluetooh app "BlueNRG" doesn't appear the "BlueNRGChat" with the cube and the other parameters.
Some times its appear, but when I connect to it says something like "No valid characteristic found. Wrong firmware?..."
If someone could help me I really appreciate it because it is really frustrating than following the guide provided by ST it doesn't work.
Thank you,
Alex :)
2018-09-13 4:04 AM
Did you achieve reasonable communication between the two boards? Sometimes you need to resolder the solder points to set it up on different pins.
Take a scope and look at the SPI communication pins, if they show reasonable activity (NSS, CLK, MISO, MOSI). If not, your pin allocation is wrong.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.