How to compile BlueNRG2 program in Linux.
Trying to compile with the arm-none-eabi toolchain always shows the following error.How to solve these.
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
Trying to compile with the arm-none-eabi toolchain always shows the following error.How to solve these.
Hi,i have a BlueNRG eval board and want to develop firmware for it. I installed the STSW-BLUENRG1-DK and found no example code. Where can i find it instead?
Hi:I have done something wrong, as i write in title, i update IDB04A1 with IDB05A1 firmware. And now, IDB04A1 can't work now, is there anyone can help me? thanks
I've had intermittent success at flashing the firmware provided with the DK for the BlueNRG tile (STEVAL-BCN002V1) when attached to the host board. I can see the image file loading on to the device memory followed by a successful verify and sometimes...
HI, while learning how to use IDB05A1 shield with nucleo n053r8 I've stumbled over a problem. I've modified SensorDemo_BLESensor-App (from package X-CUBE-BLE 1.4.40) code to create my own server with 2 characteristics:/** * @brief Add the SW Featur...
I am trying to create a BLE mesh project for flashing the BlueNRG 2 board. For this purpose I have downloaded the ST BLE mesh software version 1.07. Then I modified an already working project for the BlueNRG 2 with a working startup and linker file. ...
I have tried putting the device_id[4], PAC[8], Offset[4], Private_key[16]. Where can I find information on this ? Thank you
Good day!The question is:What temperature and for how long time I can heat BLUENRG-132 after programming without breaking the data ? In the experiment, data is saved after soldering. But, I want to understand where this is written in the documen...
Hello,we have developed some custom boards with S2-LP transceiver and BALF-SPI2-01D3 balun coupled. We notice a non-linear behaviour between the output power set to s2-LP and the measured output. By direct connection between signal analyzer and S2-LP...
Hi We are using BlueNRG-MS IC for BLE communication, in that we are facing issue with Balun filter IC package. BALF-NRG-01D3 /02D3 having CSPBGA package which we are unable to solder, so we are looking for alternate package or any alternate method f...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.