Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to transmit data when reading characteristic?

Hi,I was wondering if it is possible to send data from client to sever when reading characteristic?In order to save memory, I am trying to have only 1 profile with 3 characteristics (Read/Write/Notify). The idea is, when the client wants to read data...

ABern by Associate II
  • 1786 Views
  • 3 replies
  • 0 kudos

Network Connection Troubles

Hi all,I am using a Nucleo-144 board and enabled the FreeRTOS. Afterwards i've integrated FreeRTOS+TCP sources and headers and Paho MQTT application. I created a thread to run a MQTT Echo Server but i am having troubles connecting. This is my code:st...

AGaru by Associate III
  • 1428 Views
  • 2 replies
  • 0 kudos

What combination of DK files and iOS project files would i need to log data from a STEVAL-BCN002V1 tile to an iPhone? Thanks

I'd like to select the update rate for specific sensors and create a csv file on the iPhone. Sorry this appears to be such a basic question but i am very new at embedded systems development but anxious to have even some small progress. Any effective ...

RGupp by Associate II
  • 1374 Views
  • 2 replies
  • 0 kudos

BlueNRG2 - which call back? for write characteristic

i am writing an andriod app, i am wondering which call back of BlueNRG2 will respond after the following codes of app? BluetoothGattService gattService =bluetooth_gatt.getService(java.util.UUID.fromString(serviceUuid));BluetoothGattCharacteristic gat...

ann by Associate II
  • 865 Views
  • 1 replies
  • 0 kudos

How to configure I2C connection in BLE Mesh

I want to create a mesh in which every node (BlueNRG 2) share some sensor measurements to each other. The measurements should be transmitted over an I2C connection from a sensor module. My Problem is now that I can't configure a working I2C connectio...

EBozb by Associate II
  • 6030 Views
  • 13 replies
  • 0 kudos

cannot initialise target MCU on STEVAL-IDP005V1

I am using STEVAL-BFA001V1B evaluation kit where I am trying to initialize the MCU on sensor board present in the kit. I have connected ST-LINK/V2-1 programmer/debugger to the sensor board via an adapter board present in the same kit. The ST-LINK/V2-...

Chandu by Associate II
  • 623 Views
  • 0 replies
  • 0 kudos

How to config the STUSB4700 with 20V/5A channel

I would like to use the STUSB4700 for a powerbank application which can deliver 100W.In datasheet it says that the STUSB4700 can deliver 100W (20V/5A) But the factory configuration is only 20V/3A and it is possible to change it over I²C to 20V/5AThat...

jebert by Associate
  • 1383 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.