2019-11-19 5:49 AM
Hello,
I want to add acknowledge funtionality to the Mesh Lighting demo from ST.
What do I have to do to activate this and which funtion do I need to call to send an acknowledge-signal?
Also for visibility, I'd like to have a LED flash when the sending node receives an acknowledgement-signal is there a possibility to process those signals?
Thanks in advance
2019-12-18 9:44 PM
When using the Android/iOS "ST BLE Mesh" App, kindly go to the menu on left side of the App
Switch ON the button for acknowledgement
for board to board communication, kindly use the STSW-BNRG-Mesh V1.09
You can play with the communication by enabling the acknowledgement during the packet sending. There will be status callback when the acknowledgement is received
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.