2020-04-11 10:51 PM
请问BLUENRG1能够输出两路�?�控制的PWM�?�?最好是能够控制PWM的开�?�关闭,PWM的�?�空比。我�?试�?作定时器在工作模�?1和1a下工作,Txen都无法控制输出的开�?�关闭,是�?作方法�?对�?�?
2020-04-16 10:34 PM
Yes. Two PWM sources (PWM0 and PWM1) can be configured independently.
Please refer to MFT/PWM_SW sample in DK.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.