Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

hi, We have RS-485 with ST1480. we need 1kV surge protection. We use TVS and serie resistor in front-end. surge pulse higher then absolute rating. Will chip survive this. regards

When surge will be done the lab, they will surge at 1kV so every TVS can get (1000-31)/80 = 12A in theory. As 1A gives already 19V this is also above absolute ratings, 12A will be close to 28V.absolute rating inpût is 14V. for a quality product: can ...

DScho.1 by Associate
  • 950 Views
  • 0 replies
  • 0 kudos

S2LP CLI problems

I am using a STEVAL-FKI433V2 to try to create a packet sniffer. The standard on-board software is clearly capable of working with the supplied Python GUI to configure the radio and listen for packets. I have been attempting to send commands to the de...

unicycle by Associate III
  • 769 Views
  • 0 replies
  • 0 kudos

USB-PD Core Stack

Document UM2552 does not mention Fast Role Swap, Does STM USB-PD core stack library support FRS? If it does, anyone have more information about FRS in USB-PD core stack?Thanks

AZhou by Associate II
  • 1033 Views
  • 1 replies
  • 0 kudos

BlueNRG-1 high consumption in low power mode

Hi!I'm using BlueNRG-1 to beacon some messages.I tested a simple scenarious:100ms advertising messagesAdvertising with no connections allowed (ADV_NONCONN_IND)disable all GPIOsdisable debug printf and UARTI use the BLE_BEACON sample code with SDK 3.2...

0693W000001pVOAQA2.jpg 0693W000001pVOZQA2.jpg
uilter by Senior
  • 1081 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.