2020-05-28 4:22 AM
When surge will be done the lab, they will surge at 1kV so every TVS can get (1000-31)/80 = 12A in theory. As 1A gives already 19V this is also above absolute ratings, 12A will be close to 28V.
absolute rating inpût is 14V. for a quality product: can the device safely accept this surge above absolute ratings without influencing lifetime of the chip or do we need to select another chip with a common mode with higher than the surge or is the surge no issue due to short time and/or the extra resistors of 10R.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.