Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Modified Attribute Data is not available for all characteristics after migration from expansion board IDB05A1 to BNRG2A1

I'm a not experienced student who has to deliver his thesis in a given time frame. I developed an Android app which has to send data as a client to a Nucleo-STM32F411RE server via Bluetooth. First I used the BLE expansion IDB05A1 where I have been ab...

JMüll.1 by Associate II
  • 827 Views
  • 0 replies
  • 0 kudos

I want to use the en.x-cube-subg1_firmware for the X-NUCLEO-IDS01A5 (based on SPSGRF-915) expansion board. I'm a novice and struggling to identify hardware specific files adaptations vs the example project (for example STM32L152RE-Nucleo)

(I think I posted this in the wrong location initially. Reposting here )I am wanting to use stm32L476rg - a nucleo decelopment board that does not include SPSGRF. I am working on learning to communicate via SPSGRF from the nucleo to the STM32 IOT di...

FRozy.1 by Associate II
  • 1235 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to get the provided sample apps (Sensorapp and sampleapp) running on a Nucleo-STM32F411RE with a X-Nucleo-BNRG2A1 expansion.

I try to get the sample app and the sensor app running on a Nucleo-STM32F411RE together with a X-Nucleo-BNRG2A1 expansion. I configured everything as it was described in the corresponding docu. But I was not able to get it running. The device does no...

JMüll.1 by Associate II
  • 1401 Views
  • 1 replies
  • 0 kudos

migration from MX25L512G to MT25QL256ABA8ESF

I used disco board stm32f769i in external flash application and it works well then I used the same microcontroller type with another external flash module  MT25QL256 and the written data is corrupted .I think it is configuration problem so what the p...

GMoha.1 by Associate II
  • 2491 Views
  • 2 replies
  • 0 kudos

STUSB1602 Full Register Description Missing

I don't want to use the provided SW library for the STUSB1602, it's far too complicated for my application and I'm using a different MCU.The datasheet only has a register overview, the software doesn't seem to have any info and there aren't additiona...

BLUE-NRG-232 DC-DC converter modes

We are using BLUENRG-232 in one of our low cost designs. On page 138 of the datasheet, we can see two DC-DC converter configs. For cost savings, we would like to go with non-active DC-DC converter config. However, there isn't much info available abou...

SK.10 by Associate II
  • 2984 Views
  • 6 replies
  • 0 kudos

Addressing SPIRIT1 SPSGRF-915 Packet Loss

My project involves using two SPSGRF-915 RF Transceivers (one acting as a transmitter while the other as a receiver all the time). I observe some degree of packet loss using a debugger window connected to the receiver node, and a Logic Analyzer conne...

RrW1 by Associate III
  • 988 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.