2020-10-01 5:53 AM
Hello everyone.
Can I make a STDC14 connector on BLUENRG-M2SA?
I want to use VCP function through STLINK-V3SET.
Do you have the following Pin assignment?
STDC14(Pin No.)_(Description)_>>>_BLUENRG-M2SA(Pin name)_(Pin No.)
STDC14_01___Reserved__________>>>___NC______________NC
STDC14_02___Reserved__________>>>___NC______________NC
STDC14_03___T_VCC_____________>>>___VDD (to Vin)____VDD
STDC14_04___T_JTMS/T_SWDIO____>>>___JTMS-SWTDIO_____Pin-13
STDC14_05___GND_______________>>>___GND_____________GND
STDC14_06___T_JCLK/T_SWCLK____>>>___JTCK-SWTCK______Pin_12
STDC14_07___GND_______________>>>___GND_____________GND
STDC14_08___T_JTDO/T_SWO______>>>___???_____________???
STDC14_09___T_JRCLK/NC________>>>___NC or BOOT ???__NC or Pin-07 ???
STDC14_10___T_JTDI/NC_________>>>___NC ???__________???
STDC14_11___GNDDetect_________>>>___GND_____________GND
STDC14_12___T_NRST____________>>>___RESETN__________Pin-19
STDC14_13___T_VCP_RX__________>>>___TXD_____________Pin-10
STDC14_14___T_VCP_TX__________>>>___SPI_CS1/RXD_____Pin-11
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.