Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

St BlueNRG2 M2sA programing Error

I have ST EVAL -IDB008V1M board , i trying to load DTM Uart image (it Acts like a Network Mode) using st link utility and I geeting Error , i uploading Error image , the mode of programing will Be SWD , kindly help me out to the DTM image on the Boa...

mkuma.1 by Associate II
  • 955 Views
  • 0 replies
  • 0 kudos

Sample project for X-NUCLEO-S2915A1 using Contiki/6Lowpan available for simple UDP sender, receiver, sniffer and edge router. Is there any other sample project from STM I can refer?

I am working on a project to create a star network between a router to a number of sensors over 6lowpan using Contiki. Router will pass the messages to border router. Router and border router is connected to main power, while sensor is battery power...

AJama.1 by Associate II
  • 816 Views
  • 0 replies
  • 1 kudos

HAL_I2S_TxHalfCpltCallback and HAL_I2S_TxCpltCallback are not called on a 50:50 duty cycle as expected when using a circular buffer to I2S.

I am outputting audio over I2S at 8k with a 128 sample buffer. I was getting timing issues so I turn on an LED on the Half way callback and turn it off on the complete callback. I expect a 50% duty cycle. But I get the output below on my scope. Anyon...

0693W000004K6E5QAK_image.png
RAdam.1 by Associate III
  • 3277 Views
  • 4 replies
  • 0 kudos

Resolved! P-NUCLEO_USB002 serial debug output

I am currently working on a P-NUCLEO_USB002 board to develop a PD solution. It seems the serial debug output is playing up. I set the USB_CLI already but it just give me some garbage data. I double checked the baudrate and it seems ok. Is anyone has ...

HWong.2 by Associate
  • 1272 Views
  • 1 replies
  • 0 kudos

how to calculate blue nrg stack usage size.

I am using the BLUENRG-M2SP ble chip set , i created the 2 services ,there services are Primary Services 1. first service has the 3 characteristics and Second services has the 5 characteristics , if i add third services , i am getting Lack of Memory ...

mkuma.1 by Associate II
  • 779 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.