Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

WatchDog Timer, STWD100, manufacturing tolerance of Watchdog TimeOut Period (tWD) for the 1.6sec variant

Hello Sir/Madam,Product PN: STWD100xY.Problem: The problem is not with the actual product itself, but with the datasheet. The existing datasheet makes it very difficult to determine if the product is suitable for our application. For the value for ...

0693W000006ElmTQAS.jpg
FBaro.11 by Associate II
  • 929 Views
  • 0 replies
  • 0 kudos

TB TIMING

Hello people , we need some help from ST for solving the ST7538-Q interfacing with SPI .I don't even no where I have to ask the question .currently I am working in powerline communication using st7539-q and we are trying to communicate ST7538...

Rectifier by Associate II
  • 1306 Views
  • 0 replies
  • 0 kudos

When OTA and bonding both features are enabled, the bond information gets erased from flash each time I disconnect from the device. Any suggestions on this?

I am using BLE Chat application where I have added the bonding feature. When I don't use OTA, I can connect to the device and bond it and the bond information stays even after reconnecting to the device.But when the OTA is enabled, once I connect to ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.