2020-12-04 2:40 AM
Hello,
I have two X-Nucleo-BNRG2A1 demo board, with Nucleo Board, working fine with the SampleApplication of the X-CUBE-BLE2.
The two module pair correctly, one being the Master, sending message to the slave.
I would like now to use another device to connect to the X-Nucleo-BNRG2A1. I can see the bluetooth one the other device, but when trying to connect, it ask for a Key.
What is the Key, or how to read it? Is there a way to enable Key free connection?
Thank you
Solved! Go to Solution.
2020-12-04 8:54 AM
Hello,
Here is the solution:
To change the authentification to use Pin code, add the following in the module initialisation:
ret = aci_gap_clear_security_db();
if (ret != BLE_STATUS_SUCCESS)
{
PRINT_DBG( "aci_gap_clear_security_db failed: 0x%02x\r\n",
ret);
return ret;
}
uint8_t Bonding_Mode = 0; /* No Bonding */
uint8_t MITM_Mode = 0; /* MITM prottttection not required */
uint8_t SC_Support = 0; /* SC IS NOT Supported */
uint8_t KeyPress_Notification_Support = 0; /* Keypress not supported */
uint8_t Min_Encryption_Key_Size = 0x07; /* Minimum encryption key size */
uint8_t Max_Encryption_Key_Size = 0x10; /* Minimum encryption key size */
uint8_t Use_Fixed_Pin = 0; /* Use Fixed Pin for pairing */
uint32_t Fixed_Pin = 0x0001E240; /* Pin 1234546 */
uint8_t Identity_Address_Type = 0; /* Public Identity Adddress */
ret = aci_gap_set_authentication_requirement( Bonding_Mode,
MITM_Mode,
SC_Support,
KeyPress_Notification_Support,
Min_Encryption_Key_Size,
Max_Encryption_Key_Size,
Use_Fixed_Pin,
Fixed_Pin,
Identity_Address_Type );
if (ret != BLE_STATUS_SUCCESS)
{
PRINT_DBG( "aci_gap_clear_security_db failed: 0x%02x\r\n",
ret);
return ret;
}
2020-12-04 8:54 AM
Hello,
Here is the solution:
To change the authentification to use Pin code, add the following in the module initialisation:
ret = aci_gap_clear_security_db();
if (ret != BLE_STATUS_SUCCESS)
{
PRINT_DBG( "aci_gap_clear_security_db failed: 0x%02x\r\n",
ret);
return ret;
}
uint8_t Bonding_Mode = 0; /* No Bonding */
uint8_t MITM_Mode = 0; /* MITM prottttection not required */
uint8_t SC_Support = 0; /* SC IS NOT Supported */
uint8_t KeyPress_Notification_Support = 0; /* Keypress not supported */
uint8_t Min_Encryption_Key_Size = 0x07; /* Minimum encryption key size */
uint8_t Max_Encryption_Key_Size = 0x10; /* Minimum encryption key size */
uint8_t Use_Fixed_Pin = 0; /* Use Fixed Pin for pairing */
uint32_t Fixed_Pin = 0x0001E240; /* Pin 1234546 */
uint8_t Identity_Address_Type = 0; /* Public Identity Adddress */
ret = aci_gap_set_authentication_requirement( Bonding_Mode,
MITM_Mode,
SC_Support,
KeyPress_Notification_Support,
Min_Encryption_Key_Size,
Max_Encryption_Key_Size,
Use_Fixed_Pin,
Fixed_Pin,
Identity_Address_Type );
if (ret != BLE_STATUS_SUCCESS)
{
PRINT_DBG( "aci_gap_clear_security_db failed: 0x%02x\r\n",
ret);
return ret;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.