Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! S2-LP packet loss and DMA Rx infinite loop

Hello,I use two X-NUCLEO-S2868A2 board with blueNRG-2 with BlueNRG-1_2 DK 3.2.1 and S2-LP_DK_1.3.2I use following RF configuration :#define MODULATION_SELECT MOD_2GFSK_BT1 #define DATARATE 50000 #define FREQ_DEVIATION ...

0693W000008wyDrQAI.png
AndyR1 by Senior
  • 1224 Views
  • 3 replies
  • 0 kudos

I'm doing a project with a steval-idb008v2 and I have a doubt due to a small note. Can the steval-idb008v2 be reprogrammed with a code created specifically by the user?

the note says this: The STM32L microcontroller on the board is not intended to be programmed by users. ST provides a preprogrammed firmware image for the sole purpose of interfacing BlueNRG-1, BlueNRG-2 to a USB host device.

ASpar.1 by Associate II
  • 902 Views
  • 1 replies
  • 0 kudos

S2-LP / FKI433V2 is receiving garbage data from 433Mhz ASK Manchester Encoded 9.6KBaud transmitter using S2-LP DK GUI.

 I have tried setting the MANCHESTER_EN register and a huge combination of data rates etc in order to get some sensible data in the S2-LP GUI, but nothing is consistent or representative of the data I expect to see.I can see the data correctly using ...

0693W000008yBlyQAE.png
CKild.1 by Associate
  • 918 Views
  • 1 replies
  • 0 kudos

STMF446RE nucleo I2C interface does not work. This maybe a wery dumb question but how do i get my I2C to work? the initialization is created using cubeMX, after that i am just using the hal function HAL_I2C_Master_transmit().

So the details of the configuration are: i am using I2C3 peripheral with the clock speed of 100kHz the pins are set to open drain no pull up no pull down. I am also using external pull up ressistors.I have already checked the internet for a solution ...

BMave.1 by Associate
  • 794 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.