Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST67W61 pass-through mode

Hello, does ST67W61 module support pass-through mode?   I have an application based on a third-party IP stack and it would be a pain to rewrite it all with AT primitives. A far simpler solution would be replacing low-level calls to transmit and recei...

Resolved! X-CUBE-ST67W61 interface

  I am planning to have my application interface with the service API of the X-CUBE-ST67W61 Software package. How does the shell utility interface with the Service API? Is the communication interface through a queue?

X-CUBE-ST67W61 architecture.jpg

S2-LP: Minimal deviation for GFSK

Hi everyone!We are trying to launch the GFSK reception on S2-LP in the basic mode. We have noticed that by reducing the deviation to 10 kHz most of the received packets gets discarded and even those accepted have at least 2-3 bits of errors. This beh...

Resolved! ST67W611M1 wrong data received through SPI

Dear all, I'm trying to control ST67W611M1 wifi module by using a linux host chip. After flashing the newest firmware I reset the module to SPI mode. Some logs can be received through the uart interface and the SPY_RDY pin is drived to high level. Bu...

VL53L8CX I2C with ESP32

Hello,I wanted to share about the VL53L8CX sensor and it's I2C.I have been using a lot of VL53L sensors (5CX, 1X) and now the 8CX.It always used to work super easily but with the VL53L8CX I cannot seem to make it work. Running an I2C scan doesn't det...

ST KNX waveform reflection

I created a KNX communication module using ST KNX, but when the KNX Bus voltage is transmitted, the waveform is ringing, resulting in a communication error. I am using the recommended value of 68 Ω for the external resistor RTX on pin R68. Please giv...

arakawa by Associate
  • 1248 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.