Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Questions about Bluenrg-2N

Hello I'm in the development of the bluetooth communication between two bluenrg-2n devices. The bluenrg-2n are connected with stm32f405 through SPI. I'm not new in stm development but new in bluetooth communication. I've already done the init process...

Resolved! I2C1 ACK is not getting enabled in stm32f446re

I have configured the GPIO for I2C1(Alternate function 4) and enabled the Clock for I2C1. After that I am trying to enable the ACK. but not able to enable that.. Also tried for I2C2 and I2C3 facing the same issue.//enable the clock for the I2C periph...

PK by Associate II
  • 3030 Views
  • 6 replies
  • 0 kudos

Do I need more than one button on my device?

I have a simple project I am trying to implement using BLUENRG2-M2SA. It will connect with a user over BT and download a timer length. Then it will run the timer and blink lights when the timer counts to zero. The user then acknowledges the lights...

GGibb.1 by Associate II
  • 1717 Views
  • 2 replies
  • 0 kudos

ST-LINK V3 VCP "backpowers" board

Hello,I'm developing a board with the BlueNRG-M2 module. I'm also using an ST-LINK V3 with uVision to debug/program. I'm also using the VCP made available by the ST-LINK V3 for some good old fashioned printf telemetry. The VCP is connected through...

svcguy by Associate III
  • 3292 Views
  • 3 replies
  • 0 kudos

Getting extra bits in received message.

Trying to build a 433 MHz sniffer based on SDK example "SDK_Sniff_B.c". Im sniffing messages from TPMS sensor and get them on my PC with RTL-SDR. In the message parsed on PC I can read ID of sensor which goes right after sync word. With the help of U...

ATet.1 by Associate
  • 1233 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.