2021-06-06 3:33 AM
Hello I'm in the development of the bluetooth communication between two bluenrg-2n devices. The bluenrg-2n are connected with stm32f405 through SPI. I'm not new in stm development but new in bluetooth communication.
I've already done the init process of µC and bluenrg-2n. Now I'm little confused, whether I should care about the bluetooth process of bluenrg-2n, such as scanning, connection and pairing. If i should, which functions I should use? If not, how should I establish the connection and configure the device which I want to send data or receive data?
Are there some references or manual I can refer to?
Thanks,
Qiyuan
2021-06-07 6:50 PM
Please try to start with
UM2667 Getting started with the X-NUCLEO-BNRG2A1 BLE expansion board:
Please refer to resources of BlueNRG-2 for SDK and documents etc,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.