Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STUSB1602 Register description

Hi, I saw this question posted two years ago without an answer. Is there a full I2C register description for the STUSB1602 or does it need to be reverse-engineered from the provided drivers? We would like to add this functionality on an unsupported...

DHarr.3 by Associate
  • 501 Views
  • 0 replies
  • 0 kudos

BlueNRG advertise while having a connection

I'm trying to create a peripheral device that allows one Bluetooth central to connect to it, this part is working. Now I want the device to re-start advertisements when a central has made a connection. The advertisements should be non-connectable one...

allard by Senior
  • 2052 Views
  • 2 replies
  • 1 kudos

Resolved! How to watchdog handler on BlueNRG-LP ?

Hello,With BlueNRG1/2, we got the WEAK_FUNCTION(void WDG_Handler(void) {}); in system_bluenrg1.c, but with BlueNRG-LP there is no wdg handler in system_BlueNRG_LP.c, so is it possible to have it in any way ?Thanks.

AndyR1 by Senior
  • 1471 Views
  • 2 replies
  • 0 kudos

The problem with BlueNRG-LP and WISE Studio

I am started to make with BlueNRG-LP based ble-project using WISE Studio IDE.I choosed BLE SensorDemo example for our project.But,When compiling the example source, WISE Studio generates makefile only with the FIXED paths such as E:/Drivers/folder an...

JHP73 by Associate
  • 2128 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.