Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST67W Internal/External CoExistence Support

Hello,I am designing a Matter/Zigbee Gateway using an STM32U5 as the host. My planned architecture includes:ST67W: Handling Wi-Fi and Thread (Matter over Wi-Fi/Thread).STM32WBA (or similar): Handling Zigbee (Matter Bridge logic).I have two specific q...

S2-LP - PQI stops RX timer at wrong channel

Greetings,I'm working on a project where S2-LP scans multiple channels and receives a packet when a valid preamble is detected. For dwell time timing I'm using the RX timer. The timer is set to 2 milliseconds and is stopped whenever a valid preamble ...

pelgrimo_1-1765266140748.png
pelgrimo by Associate II
  • 474 Views
  • 1 replies
  • 0 kudos

Resolved! Command system for ST67W611M1.

Hello,Where can I view the commands sent and received from the ST67W611M1 using the SPI and UART? The datasheet doesn't provide this information. I couldn't find any other documents describing the command system on the ST67W611M1 page.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.