2025-06-27
9:09 AM
- last edited on
2025-07-08
7:51 AM
by
Lina_DABASINSKA
Just received my X-NUCLEO board and I am trying to discover what the default firmware is on the shipped boards? The getting started guide appears to suggest one needs to program the module.
Sid
Solved! Go to Solution.
2025-06-30 3:34 AM
Hello,
Yes, there is a latency between the binary we were able to flash in factory and the binary fully featured and in line with X-CUBE-ST67W61 released for MML.
So, please, follow the getting_started procedure for the current period.
Thanks,
Benoit
2025-06-30 3:34 AM
Hello,
Yes, there is a latency between the binary we were able to flash in factory and the binary fully featured and in line with X-CUBE-ST67W61 released for MML.
So, please, follow the getting_started procedure for the current period.
Thanks,
Benoit
2025-07-10 1:51 PM
I hope you can help a little more.
I have ported the NCP_Loader to run on my Nucleo-F411RE, however, I do not seem to be able to flash the ST67W61M1 using STM32CubeProgrammer.
With the Nucleo in "flash" mode I see the CHIP_EN and BOOT signals operate as described. When I try to connect the programmer, it gives an error that it timed out trying to connect.
If I observe the Nucleo UART_TX to the expansion board I see a single byte, 0x7F. I believe this is the programmer trying to get the attention of expansion board. I never see a reply.
Any pointers you may be able to give would be much appreciated.
2025-12-03 2:38 AM
Can we use st67w61m1 with stm32f401re ? and if yes what is the procudure to do it?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.