2025-12-04 12:11 AM
Hello,
I am designing a Matter/Zigbee Gateway using an STM32U5 as the host. My planned architecture includes:
ST67W: Handling Wi-Fi and Thread (Matter over Wi-Fi/Thread).
STM32WBA (or similar): Handling Zigbee (Matter Bridge logic).
I have two specific questions regarding the ST67W's coexistence capabilities:
Internal Coexistence: Does the ST67W natively support concurrent operation of Wi-Fi and Thread simultaneously without external hardware arbitration?
External PTA Support: Does the ST67W expose 3-wire PTA pins (Request/Priority/Grant) to manage coexistence with an external 802.15.4 radio (e.g., the STM32WBA running Zigbee)?
Basically, I need to confirm if it supports a "Hybrid Coexistence" setup where it manages internal Wi-Fi/Thread traffic while acting as a PTA Arbiter for an external Zigbee MCU.
Thanks in advance.
Solved! Go to Solution.
2025-12-10 12:56 AM
Hello,
1/ ST67W is capable of managing coexistence between the different protocols, and in particular between Wi-Fi and 802.15.4.
Concerning 802.15.4, Thread is under development. ST67W is also Zigbee ready, but SW is not yet in development state.
-->Depending on your plannings, your complete use case could be supported by ST67W/U5 (Matter on U5) without needing an additional device like STM32WBA.
2/ There is no PTA interface available to manage coexistence with a STM32WBA.
Depending on your final use case, it could be possible to manage it at application level, although this is not coexistence.
Br,
Benoit
2025-12-10 12:56 AM
Hello,
1/ ST67W is capable of managing coexistence between the different protocols, and in particular between Wi-Fi and 802.15.4.
Concerning 802.15.4, Thread is under development. ST67W is also Zigbee ready, but SW is not yet in development state.
-->Depending on your plannings, your complete use case could be supported by ST67W/U5 (Matter on U5) without needing an additional device like STM32WBA.
2/ There is no PTA interface available to manage coexistence with a STM32WBA.
Depending on your final use case, it could be possible to manage it at application level, although this is not coexistence.
Br,
Benoit
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.