2025-02-14 9:21 AM
Hello,
I'm using BALF-SPI2-02D3 with the S2-LP chip at 433MHz.
However, my application is only for reception, and no RF transmission. What should I do with the Tx pin on the Balun? Open, Resistor to GND or Capacitor to GND?
I also need the same answer for the S2-LP TX pin.
Thank you!
2025-02-15 12:31 AM
Hi,
why not just connect as its designed to be ?
Leave open an TX might be a bad idea , if it doing anything with rf power on.
And if you only use the reception then , so no problem to have the inactive Tx connected.
2025-02-17 3:29 AM
Hi.
I won't leave it open unless recommended.
I don't want to connect the pin to avoid another source of interference and noise into the design.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.