cancel
Showing results for 
Search instead for 
Did you mean: 

BALF-SPI2-02D3 datasheet stackup: what does “35 µm + 31 µm” mean?

cehmke
Associate

I’m using BALF-SPI2-02D3 with the S2-LP at 433 MHz and have a question about Figure 13 in the datasheet.

The recommended PCB stackup shows:

  • Top plane: 35 µm + 31 µm
  • Mid layer: 31 µm
  • Bottom plane: 35 µm + 31 µm

What exactly does “35 µm + 31 µm” mean for the outer layers?

Is this:

  • base copper + plated copper,
  • finished copper thickness in ST’s stackup notation,
  • or something else?

I’m trying to choose a 1.0 mm, 4-layer PCB stackup from a commercial manufacturer and would like to match the recommendation as closely as possible.

Thanks for any clarification.

0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.