2021-07-07 2:53 AM
I see that all examples are for IAR or KEIL IDE.
Can you provide CubeIDE projects as well?
Regards,
Piotr Romaniuk
2021-07-07 7:43 PM
There are no STEM32CubeIDE projects in S2-LP DK currently.
But you may convert them in case needed.
Please refer to TrueStudio migration guide
Please also reference the post in community:
2021-07-08 4:54 AM
Hi Winfred,
thank you for the comprehensive migration guide. I found there some new information.
In general, I know the step needed for porting, but this is some extra work to be done.
It would be nice to have a version of project for IDE that is owned by ST (currently it is CubeIDE, TrueStudio is deprecated).
Of course we know advantages of IAR Workbench and KEIL IDE, but I'd rather expect that I also found in DK the example of source code that run on ST IDE.
The DK source code is 2 years old, so maybe it is good idea for ST to add project files for CubeIDE as well?
In my opinion this problem is common for many engineers that would like to evaluate Spirit2-LP chip, and the need of porting can discourage them.
Regards,
Piotr Romaniuk
PS
By the way, on which IDE were built binaries in DK?
2023-08-10 12:41 PM
Hi Piotr,
Did you manage to import the IAR project into CubeIDE in the end?
If so, do you remember how difficult it was?
Cheers!
Cris
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.