2017-05-03 2:18 AM
Hello,
My question is about BlueNRG-1 .
I want to design a about bluetooth master and slave Fixed PIN pairing.
But the Fixed PIN seems to be no effect.
Specific how should do?Thanks !
2017-05-05 1:02 AM
Dear Customer,
as example you can see the scripts: Security_PassKeyEntry_Master_Role.py and Security_PassKeyEntry_Slave_Role.py, that you can find inside last installation package.
To use fixed pin, you have to modify lightly these scripts, for example in the ACI_GAP_SET_AUTHENTICATION_REQUIREMENT command, you have to set the field Use_Fixed_Pin = 0x00 (fixed pin ) instead of 0x01 (requested pin).
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.