cancel
Showing results for 
Search instead for 
Did you mean: 

Why the VL53L1 sensor VL53L1_Dev_t object consumes 5.43KB(Kilo Bytes) RAM in api ver 1.1.37.12156 where as the same object consumes 932B in api ver 1.2.11.1840 ?

NKuma.10
Associate

Hi,

I am porting the one of legacy VL53L1 stack (STM api ver 1.1.37.12156 ) for one of the project. This stack is stable and well tested. However, i am surprised to see the RAM consumption(5.43KB) of the VL53L1_Dev_t  object. This is different in new STM api ver 1.2.11.1840 (932B). I can understand that new api might have optimized or deprecated some of implementations.

Why is VL53L1_Dev_t  object consuming RAM memory of 5.43KB? It will really help me if any change list file is available to download or can provide here.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John E KVAM
ST Employee

​In the file:

vl53l1_platform_user_config.h

is the line:

#define VL53L1_MAX_USER_ZONES               16

By lowering the number of zones, the data structure is GREATLY reduced.

What you are seeing is the result of the lower number of zones.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.