2021-07-10 1:58 PM
I have exposed both GPIO1 and GPIO2 pulled up to VDDIO with a 47 K resistor on my VL53L5 breakout. GPIO1 is used as the interrupt. What can I use GPIO2 for, another interrupt? It would be very convenient to have a date ready interrupt on GPIO1 and a threshold interrupt on GPIO2, for example...
Is there an AN describing use of these GPIOs?
2021-07-15 12:47 PM
At the moment the GPIO2 is undefined. But the firmware running in the VL53L5 is downloadable, so it's subject to change. But at moment GPIO 2 does nothing.
GPIO is an unfortunate term. GPIO1 was a GPIO until we wrote the code. At that point it was no longer a general purpose pin. It was fixed as an interrupt pin.
But the use of GPIO2 is undefined at the moment.
2021-07-15 1:16 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.